integration in Home Assistant
Dear Sirs,
I need to change the first url address to integrate the Legrand Home Plus inside Home Assistant. How can I do it?
BR,
Michele
Hi Michele,
You need to edit your application : https://mysettings.developer.legrand.com/Application/Index > application’s details. I’ll then have to approve changes
Have a good day,
Leslie – Community Manager
Bonjour, je souhaite également intégrer dans home assistant.
J’ai renseigné le client ID , client secret et subscription key.
lorsque j’installe l’intégration legrand et j’ai le message 500 internal server error.
Pouvez vous m’aider ?
Hello Damien,
Please speak in English here in order to be understood by the majority đŸ˜‰
I just validated some applications, is yours in “Approved” state ?
As far as I know, you just have to fill in provided information in the YAML file of your HA installation. If it still doesn’t work, please send me your client_id via the contact form and I’ll check in database if your application is correctly set
Have a good day,
Leslie – Community Manager
Hello michelebergo,
Could you advise me the first url for HA, is is local or public address? I would like to be sure before need help from Leslie, approve for the first url because I have same issue
Thank you so much
Best regards
Hi All,
I’m trying to integrate Legrand to HA. I use cloudflare to export my HA to internet.
I set up the Legrand application specifying the URL as https://<myPublicSite>.it that is my redirected by cloudflare to my HA. I applied the required configuration to HA but when I try to add the Legrand Home control it redirect me to an URL that contains a URL different from the one that I specified.
https://partners-login.eliotbylegrand.com/authorize?response_type=code&client_id=187e1334-9527-464c-ba0c-b097e303a387&redirect_uri=https://my.home-assistant.io/redirect/oauth&state=…..
I didn’t specified my.home-assistant.io anywhere.
I tried to change it with my public site and I have been asked to allow the access, but if I accept I get a 404
Could you please help me on that?
Hello Grégory,
I have also to manually re-approve applications updates (you can follow its status in your application’s interface)
I just re-validated it
Have a good day,
Leslie – Community Manager
Hello Max,
For your Works with Legrand developer application, the best in my opinion is to create a new one in order to go on a “clean” configuration and to be sure that the problem doesn’t come from here
If you didn’t specify at all my.home-assistant.io as one of the reply url, it’s probably something stored in your Home Assistant configuration (maybe in the .yaml file or somewhere else) ? As it’s a third-party service I can’t bring much help if it comes from here, best is to ask to HA community via their forum
Have a good day,
Leslie – Community Manager
Hi,
i would also like to integrate my Home + control into home assistant.
How should I proceed ?
I’ve created a subscription and I wanted to create an application but what URL should I put ?
Thanks for your help.
Regards,
Julien
Hello Julien,
Here is a post telling to use the URL of your Home Assistant instance : https://github.com/home-assistant/home-assistant.io/issues/17337
In a more general way, it’s an URL needed to do a redirection to a webpage to accept consent to the third-party service. So, any other one should make the job
Have a good day,
Leslie – Community Manager
Hi Leslie,
Thanks for the link but when I want to create the application is says that the name is not available (in the “Name” field).
What should I put here ?
Thanks for your help.
Have a good day,
Julien
You must be logged in to reply to this topic.