Forum

Browse topics, discover Works With Legrand community!

Replace Power supple My HOME legrand Кат. № E46ADCN on MEAN WELL DRC-60B

Hi guys.

If so power supple my home legrand Кат. № E46ADCN is broken and you need to replace it quickly then:

Replace the E46 Power supply – input 230 Vac, output 27 Vdc SELV – maximum consumption 450 mA or 1,3A – DIN rail mounted model  on the Power supply Mean Well DRC-60B, Uвых1=27.6 В, Iвых1=0…1.4 А, see the connection diagram in the attached file.

It is possible to take the filter elements from a broken power supply E46.

BR, Serg

Hello Sergey,

Fo this kind of pure hardware question, you must ask it directly to the Customer Support of your country

Have a good day,

Leslie – Community Manager

Viewing 2 posts - 1 through 2 (of 2 total)

You must be logged in to reply to this topic.