Hi all,
I’m using the v55 for a while now and am really happy with the new tilt function.
However I noted that the tilt function is not working immediately when the shutters are closed to 100% when operating from the Home+Control App/Homekit.
Only after around 50 seconds, I can hear a relay switching within the shutter switch. After that I can start tilting the shutters.
The workaround so far is to only close the shutters to 99% after which the tilt function works immediately.
(When operating with the buttons on the shutter switch directly, this problem does also not exist as the relay will switch back as soon as I press the upward button to start tilting the shutters)
Has anybody else noted this behaviour. Or did I do something wrong in the calibration process?
Thanks.