Sorry Leslie. I have not explained myself very well. The 4 way scene buttons work very well.

The automations from it are still slow but hopefully that will resolve itself in time, I had bought 1 module night and day switches for each room, hoping I could use them as triggers for the same automations at the doorway but it looks like they are global, I.e, they all do the same thing.

i have a workaround. I can use your single module snap in wireless switches to do the automations, but they have to be paired to a switched device. I am simply going to point them all at a micromodule unit which I will connect to ac power but no output and hide it somewhere. If the wireless switch has to toggle that on and off it doesn’t matter,

I was asking if a 4 scene switch will ever be available as a snap in double module for your frames. Like the wireless switches were stick on only until you released the snap in version.

lastly, as to the fan controllers, I have heavily invested in the system on the understanding that the fan controller is coming. If it does not become available I am missing a critical part of the hvac control for my house with your system.

best

 

paul