Hi Leslie and all community members,

In previous posts, I had said that my rolling shutter were working correctly with the new firmware and that I could adjust the opening percentage between 1 and 100% using the Apple Home app or the Legrand Control app.

And indeed they worked perfectly well until … this morning.

This morning when tried to open 20% of the rolling shutter of my room using the apple home app, I got a “no response” error. Then I switched to the Legrand Control APP to adjust this opening percentage and I could adjust the opening percentage like I wanted and when I switched back to the apple home app, I was not able anymore to adjust the opening percentage. Not only for this rolling shutter but for all my 9 rolling shutters that worked fine until yesterday.

Now I am facing the same issue of other community members for all my 9 rolling shutters: I just can set 3 positions, 0%, 50% and 100%

Can you check what could justify this behavior ?

This is really very disappointing !

Regards, Guilherme