configurators – are these just a resistors ?
Hello.
There is such thing as “configurators” by legrand/bticino put in 2-pin slot in various legrand devices (like videodomofons). These seem to be just a resistors with different package (my guess, don’t have these).
Does anyone know values of these resistors for 0-9 configurators?
Hi arek,
I don’t think you will find an answer here (this forum is aimed to help developers using the APIs of our connected devices)
I advise you to see it with the Customer Support of your country
Have a good day,
Leslie – Community Manager
In case anyone else looking for this information:
1- 822 kΩ
2- 680 kΩ
5 – 390kΩ
Hi Arek – did you measure those – if not is there an official Bticino reference ? I have one or two jumpers that I think have drifted and I have not got the standard spares kit (1-9) plus #SLA – I am measuring:
840k on #1
685k on #2
which looks in spec
but I suspect my issue is SLA special jumper – I am measuring 122k – this particular relay module ( it is a gate bell / entrance panel / repeater ) is not working – the relay itself seems to work when configured to other input sources. It relies on SLA. ( call panel button )
You must be logged in to reply to this topic.