Forum

Browse topics, discover Works With Legrand community!

Double remote switch binding

<p>Hi all,</p><p>I want to bind my double remote switch to respective connected switches while using them in zigbee 3.0 mode. I tried the press 3 seconds on ZR device and then 3 seconds on ZED device but I can’t understand when the bind will end up going, the left or the right remote button. even when I try once and lets say the left bind OK, then the second try will still bind again to the left and not the other button as you would imagine. what is the logic there?</p><p> </p><p>thanks </p>

Hello,

To select which side of the switch to associate, you first have to make a short push on it

To associate the left button :

1. short push on the left part of the switch

2. binding of the ZED with the ZR

  • 1. 3s push on the ZR EZ button
  • 2. 3s push on the ZED EZ button

 

Do the same think with the right button and it should work

Have a good day,

Leslie – Community Manager

<p>thank you Laslie</p><p>i tried this but after successfully binding the first light to the left button, i tried the right one and now the right button controls both lights. very strange. </p><p>this is on Z3.0 network. </p><p>now i took it off the network and connected it to legrand gateway to try and update it there because it is on verison 47 and there is an update for it.</p><p>BTW, is it enough for it to be connected to legrand gateway for OTA update or it has to be binded to a connected device as well?</p>

Hello,

Normally yes, if the switch is connected to the Legrand gateway network, the OTA update will be done automatically

Have a good day,

Leslie – Community Manager

<p>for 3 dasy now it is connected to legrand gateway and still on 47. i tried to take out the battery and reinsert it to trigger the request for OTA on boot but still not working. any more sugestions?</p>

Hello,

Really strange, I see that the firmware update was successfully done but the NLD is indeed still in v47 :

Last Setup
12/10/2025 10:47:33
Last Update
12/10/2025 10:48:05

I asked the team, a solution can be to perform a push on the push-button (up and down) and hold it for around 7 to 10 seconds until the LED flashes in magenta (the switch must be in the Legrand gateway network during the process)

Can you please try this ?

Have a good day,

Leslie – Community Manager

<p>i tried this and got the yellow/orange (not sure) for few seconds and then it turn off.</p><p> a solution for what exactly is that? for the FW version?</p>

Hi,

Seems like it’s 20 seconds to hold the button and not 7. They sent me a video to show the process : https://we.tl/t-kKf5hP7Dy7. Can you re-try ?

Have a good day,

Leslie – Community Manager

<p>Thank you</p><p>so i did it like shown, but for me it first turn yellow light after 7 seconds and then continue for 20 and it blinked 3 times magenta. <br />what should happen now? When should i expect it to uodate? Because it is still 47…</p>

<p>It worked!</p><p>Thanks Leslie 🙂</p>

Viewing 10 posts - 1 through 10 (of 10 total)

You must be logged in to reply to this topic.

Information

9 replies
2 participants