F461 – MyHOME Server for third party integration
Hello Dario,
We have a dedicated documentation for MyHOME system available here : https://developer.legrand.com/local-interoperability/#PDF%20documentation
Have a good day,
Leslie – Community Manager
So the new F461 uses OWN? Do you know the OWN commands for the new F429D and F429G (DALI2 dimmers and gateways)?
Yes I confirm it uses OWN protocol
All the WHO 1 document is about Dali2 commands : https://static.developer.legrand.com/files/2024/05/WHO_1.pdf
Have a good day,
Leslie – Community Manager
Hi Leslie,
If F461 uses OWN, how it could work with Savant, as stated in the product webpage (https://catalogue.bticino.com/product/smart-home-solutions/my-home—home-automation-system/integration-and-control/BTI-F461-EN) if OWN needs two communication sockets, and Savant can’t do it? We had this problem with the previous gateways, Legrand knew that. Now i have a F461 to try to develop a driver for Savant integration, since someone stated that now it’d be possible, but if nothing changed, i don’t think it will. Is it not possible to use MyHome_Up or even Netatmo API with it?
Thanks
Hi Fernando,
I created an internal ticket to ask the question to the teams. I’ll tell you once I have their answer
Have a good day,
Leslie – Community Manager
Hello Fernando,
I just received the answer from our internal support :
Since for intergration with OWN two sockets are required and Savant cannot do it, we have made request to remove from documentation and product webpage the compatibility with Savant.
For the question “Is it not possible to use MyHome_Up or even Netatmo API with it?” :
- MyHomeUP is no more available and F461, like F460, EOS and native MHS1, is not compatible with it.
- Netatmo API are not available since F461 does not use Netatmo cloud because it is designed to use third-party apps instead of H+C.
Have a good day,
Leslie – Community Manager
We are connecting successfully to a F461 but having a problem for monitoring.
The command session using *99*0## is ok, we can command lights, for example, while keeping it alive between 30 secs.
But the monitoring session, opened by sending *99*1## on connection, does not bring anything from the server, not a single message (after succesfully connected). And it should bring ALL of the feedback of what’s happening in the BUS.
F461 running firmware 1.2.11.
Could someone check this problem?
You must be logged in to reply to this topic.