Forum

Browse topics, discover Works With Legrand community!

Legrand Excel Life Smart Dimmer only turns on with long press

I have a Legrand Excel Life Smart Dimmer (EWNDIM) that I have paired to my own Zigbee network (Home Assistant with a Sonoff Zigee coordinator).

I’ve paired it successfully and I can control everything through Home Assistant: Light on/off, brightness level.

On the switch itself I’m having a problem where I can turn the light off with a regular short press, but to turn the light on I have to do a long (~2s) press. If I just do a short press, nothing happens.

Once the light is on, long pressing works fine for adjusting the brightness and then a short press turns off the light.

Is there anything I can do to be able to turn the light on with a short press of the switch? Is this the normal behaviour for the dimmer?

Thank you

  • This topic was modified 1 year, 1 month ago by Michael.

Is there a value I can write to

Cluster: 0xFC01

Attribute:  0x0000

?

It appears to have something to do with the dimmer mode? It’s currently set to 0x0101

Hello,

Here is the answer from our Zigbee expert :

The attribute id are 0x1 and 0x2 (do not use at all 0x0)

EDIT : added table in the attachment

 

Hoping it answers your question,

Have a good day,

Leslie – Community Manager

Images:
You must be logged in to view attached files.

<p>I have this issue too but there is no answer here?</p>

<p>Is there anything I can do to be able to turn the light on with a short press of the switch?</p>

Viewing 4 posts - 1 through 4 (of 4 total)

You must be logged in to reply to this topic.