Max light value in dimmer switch
hi
i would be nice to be able to limit the max light level in a dimmer switch depending on time of day. For example, if I turn on the light at night it will be automatically limited to 10% so it is more comfortable to the eye
thank
The best would be to have time factor as input condition for automations. Then it’s easy to set this up.
example:
if
time is between 22:00 and 6:00
light livingroom light status is ON
then
set livingroom light brightness to 20%
Matej
Viewing 3 posts - 1 through 3 (of 3 total)
You must be logged in to reply to this topic.