Forum

Browse topics, discover Works With Legrand community!

NLT / NLD OTA update process

<p>Hi,</p><p>According to NLT and NLD device Legrand specifications, </p><p>Could you please tell us:</p><p> what is exactly the expected condition to initiate themselves an OTA update process?</p><p>is there any limitation regarding battery soc?, linkage quality? any thresholds? and so on …</p><p> </p><p>Thank you by advance for you efficient answers,</p><p>Br</p><p>/olivier</p>

<p>+1 for this.</p><p>please give us any info about how to update the battery remote switches. especially using zigbee 3.0 mode. all my device are updating but only battery ones are timing out and don’t start the update process </p>

Hello,

Here is the answer from the teams :

“If the remote switch has a battery with a voltage greater than 2100 mV, the update should work. In theory, remote controls in a ZB3 network ask for an update at boot, and every 12 hours.

With a Zigbee capture we’ll be able to determinate if the ZED is faulty or not”

Have a good day,

Leslie – Community Manager

<p>Hello ,</p><p>yes please help us to understand whats wrong because  OTA upstate stalls.</p><p>log file attached.</p><p>first analysis from  my side;</p>

  • Request and response sequence for image blocks is fully consistent and correct.
  • No block-level transfer errors, mismatches, or anomalies.
  • Stall is caused by missing manufacturer-specific protocol handling after block transfer (i.e., Zigbee2MQTT does not handle the Legrand-specific post-OTA command, so the device never completes the update).

<p>Failed to parse frame: Error: Cluster ‘manuSpecificLegrandDevices’ has no command ‘9’</p><p>what is it?</p><p> </p><p>please advise us</p><p>thank you for supporting us</p><p>Have a nice day</p><p>/olivier</p>

Hello Olivier,

Can you please send your .txt file via the contact form ?

Have a good day,

Leslie – Community Manager

<p>hello,</p><p>cant do that, there is an issue with contact form when sending…parserror</p><p>""</p><p> </p>

Hmm strange, there is a global Azure issue currently. It’s maybe linked to this

You can write me directly on ww-sm-contact-workswithlegrand@legrand.com

Have a good day,

Leslie – Community Manager

Hello,

Here is the feedback from the team :

“The 9 command of this cluster allows our gtw to pair 2 Zigbee devices. It’s Legrand specific, their gtw must ignore this frame. But I don’t think that it avoids the update to be done.”

@olivier the logs you sent are the ones from your gateway but not a wireshark Zigbee capture. So it’s complicated to help with these logs. Can you send a wireshark capture ?

Have a good day,

Leslie – Community Manager

<p>Hi you’re right,</p><p>please find attached “simple toggle switch” log in  PCAPNG format file showing  a stalls when initiates an ota update (Address 0x1078)</p><p> </p><p>Thanks</p><p>Olivier</p>

<p><p>Sorry to come on that one, but I didn’t find a way to open a new topic<br /><br />I’m currently trying to OTA update a Cable Connect from version 13 to 39.</p><p>The OTA update went very nicely and after old blocks sent, I got the Upgrade End Response.</p><p>Unfortunatly when I query Cluster 0x0000 Attribute 0x4000 I still get 0x0013 as the version <br /><br />The firmware I used is : https://static.developer.legrand.com/files/2025/09/1021-0015-002745ff-NLC.zip</p></p><p> </p><p>Could be related to Legrand-specific post-OTA. Where could we find the specifications ?</p>

Viewing 10 posts - 1 through 10 (of 10 total)

You must be logged in to reply to this topic.

Information

9 replies
4 participants