Forum

Browse topics, discover Works With Legrand community!

Recent firmware upates

Hello Leslie,

Are you able to provide change logs for the firmware updates published on March 5th. It looks like these were updated:
NLF: 74
NLL: 61
NLD: 45
NLTS: 30
NLIS: 26
NLIV: 27
NLH: 14
NLY: 5

 

Thanks!

 

Hello Steven,

In the attachment a part of the changelog. For the 3 following the “readable” changelogs are missing, but in a nutshell :

NLIS – 26 : bug fixes and zigbee improvements

NLIV – 27 : bug fixes and zigbee improvements

NLY – 5 : first Production version for the tri-phase ecometer, so no changelog for this

 

Have a good day,

Leslie – Community Manager

 

 

Images:
You must be logged in to view attached files.

Thanks Leslie.

Hi Leslie,

Did any of these firmwares get pulled from deployment via the Legrand Gateway? I was able to get one of my NLD devices to pull 45 the other week, but now new devices are only getting 44.

 

Hello Steven,

Yes, it seems like for now v.44 is pushed instead of the v.45 which had minor issues. They started to deploy this week NLD – 47 in Production to fix these problems

Have a good day,

Leslie – Community Manager

Thanks for the confirmation Leslie. I guess I’ll just wait for 47.

Hi Leslie,

I see that NLD 47 has been available on the Legrand Gateway for a couple weeks; any idea when it’ll be available for download?

Thanks

Hi Steven,

I have a meeting with the teams on this subject in 2 weeks, I’ll then update all firmware at once

Have a good day,

Leslie – Community Manager

Viewing 8 posts - 1 through 8 (of 8 total)

You must be logged in to reply to this topic.

Information

7 replies
2 participants