Replace Power supple My HOME legrand Кат. № E46ADCN on MEAN WELL DRC-60B
Hi guys.
If so power supple my home legrand Кат. № E46ADCN is broken and you need to replace it quickly then:
Replace the E46 Power supply – input 230 Vac, output 27 Vdc SELV – maximum consumption 450 mA or 1,3A – DIN rail mounted model on the Power supply Mean Well DRC-60B, Uвых1=27.6 В, Iвых1=0…1.4 А, see the connection diagram in the attached file.
It is possible to take the filter elements from a broken power supply E46.
BR, Serg
Viewing 2 posts - 1 through 2 (of 2 total)
        You must be logged in to reply to this topic.