Netatmo wired shutter switch in local Zigbee network
Hello,
I’m struggling to setup a “Legrand with Netatmo” shutter switch (067776A) to my local Zigbee network and I’m trying the developer community to see if anyone can help 🙂
I’m integrating the shutter switch in my Home Assistant locally with Zigbee. Pairing through the reset button works well enough and I am actually able to control the shutter as intended (yay !). The problem I have is with the LED that either blinks green or stays red : I’ve been trying everything I could think of for a week and I haven’t found a way to turn it off (or even better use the “led if on” and “led in dark” features).
Another thing that I haven’t managed to do is the OTA firmware update through Home Assistant Zigbee2MQTT plugin which doesn’t seem to work (the switch doesn’t seem to accept the update).
Is there any way to properly setup the device in a local Zigbee without the “starter kit” and the Netatmo cloud that goes with it ?
Here is the “state” of the device as I read it with Zigbee2MQTT, with a firmware version :
{
"calibration_mode": "classic_nllv",
"led_if_on": "OFF",
"led_in_dark": "OFF",
"linkquality": 148,
"position": 100,
"state": "OPEN",
"tilt": 100,
"update": {
"installed_version": 2900483,
"latest_version": 3950079,
"state": "available"
},
"update_available": true,
"action": null
}
Thanks a lot,
Antoine
You must be logged in to reply to this topic.