Feedback of thermostat with third party application
Hello,
I would like to know how it is possible to get thermostat status (on or off) on third party application using OPEN SCS command. I know how to read OPEN SCS command feedback to know status of lighting (on or off) with F455.
I have a project of 350 apartments in which there are:
1. 1 x F455 gateway but NO F454 and NO MyHomeServer1
2. From 4 to 12 thermostats 067459
3. No temperature panel 3550 or 573918
4. 1 x 4 scenario controller type 573902
5. 1 x scenario module F420
Currently, it is possible to turn on or off the thermostat, control the fan speed and change the mode but I can’t get the status of the thermostat when sending a request to the gateway (server).
Would you have any solution or advise on how to do this on 3rd party application ?
Thank you.
Best Regards,
Benoit B.
You must be logged in to reply to this topic.