MyHomeserver1 and 3rd party integration
Hi all, I’m quite newbie on this forum, so please apologies in advance for any possible “gaffe”.
This is my first post after +5y (in the past I was quite active on the myOpen community forum). I’m not professional but passionate
I own a 10y old myhome plants with F454 as gateway (lights, shutters, energy, IR splits, sensors and burglar alarm), and I use Nodered on raspberry PI which works fine with F454. With this, I’ve integrated bTicino with Hue, Shelly, Sonoff, Control4, Alexa and others 3rd party devices, finally decommissioning MH200N
Now, I got a brand new MHS1 and making some test in order to see If i can update my old bTicino gateway.
My NR app does not implement HVAC password authentication with MHS1. Question: Is there anyway to configure MHS1 accepting connections from an authorized Ip address range (white list) as in the previous (F453AV, F454 or MH200N? If so, how can I set up giving that MHS1 (to best of my “poor” knowledge) has no webgui and with MyHomeUp none of this option is available.
Before posting this request, I’ve been searching for a while on the forum and I haven’t found nothing useful (assuming I’ve correctly searched). Should I have done something wrong, please apologies and drive me to the right answer.
Thank you in advance
Francesco
Hi mate,
Did you solve this?
I am in the same situation. I would need to add an IP address to this kind of “white list”.
How this can be done on the MyHome Server1?
Thank you.
Josep
Myhomeserver1 isn’t official openwebnet server as F454 and some other BTicino hardware.
This is the reason because you haven’t “Range IP” to enable not autenticated connections.
Myhomeserver1 has only HMAC autentication, and this will be removed also from new hardware version of Myhomeserver1
Bye
Sandro
You must be logged in to reply to this topic.