Forum

Browse topics, discover Works With Legrand community!

NLC Firmware Version

Hi
Before upgrade a Zigbee NLC, i have fetched this version

cluster ‘genOta’, data ‘{“fieldControl”:0,”fileVersion”:1524227,”imageType”:21,”manufacturerCode”:4129}’ from endpoint 1 with groupID 0

1524227 its 0017 so v23

i use the v31 on your website my system detect this version 2048515

The upgrade was a success

but After my zigbee composent sent me this :

‘commandQueryNextImageRequest’, cluster ‘genOta’, data ‘{“fieldControl”:0,”fileVersion”:2049023,”imageType”:21,”manufacturerCode”:4129}’ from endpoint 1 with groupID 0

this version : 2049023 its not corresponding on detected files you have an idea ?

Hello Clément,

I answer to your 2 topics at once

I asked Netatmo’s developers, here is their answer :

Currently, there is a little difference between the file version readable on the update file and the file version retrieved by the ZigBee stack. We will fix this error is the next files we’ll put online so that the 2 files will match. This being said, this has no impact on firmware and they will correctly work

Have a good day,

Leslie – Community Manager

Ok but for me and other : https://github.com/Koenkk/zigbee-OTA/issues/328

we have all same issue about the NLP v78 Firmware of your website, where we see our NLP Devices respond a error code 0x96: ‘invalid image’. debug 2023-06-12 23:40:57Error: Update failed with reason: ‘invalid image’

however the NLC firmware Works

hi

i Up the topic

Hello Clément,

I warned the teams, they planned to try to reproduce it in the next sprint starting next week. I’ll tell you once I know more

Have a good day,

Leslie – Community Manager

Hi again Clément,

I had a feedback from developers regarding NLP-78 : it correctly works on their side

Here is their answer :

Test conditions :

  • Gateway Zigbee = ZUTH lab Zigbee 3.0 certification gateway (Silab based)
  • NLP fw update from 54 to 78

Proof: Capture Zigbee in attachement.

Network key: 917455d7f02a733528fb7b8da7d613d1

network filter:  wpan.dst_pan == 0xaabb

Conclusion:

We correctly see the plug updating at the end of the capture and it launches in v.78  (frame 34532)

They can investigate more but they will need to know the start version you use to test the update and, if possible, a Zigbee capture of your OTA

You can compare with the capture I added in attachement

Have a good day,

Leslie – Community Manager

Images:
You must be logged in to view attached files.

I update from v74 (“installed_version”: 4867071, )
and v62 (“installed_version”: 4080131)

We use this version for v74
https://github.com/Koenkk/zigbee-OTA/raw/3b61e152fbdfefa00c2df4351a454b5b82734208/images/Legrand/1021-0011-4a4203-NLP-74.zigbee

and this version for v62
https://github.com/Koenkk/zigbee-OTA/raw/0bfe6a7b682fde3559b66c1d600038415868b07b/images/Legrand/1021-0011-3e4203-NLP-62.zigbee

they both dosent work

003e > v62
004a > v74
(hex to dec)

Clément,

Even from v.74 to v.78 no problem on their side

Capture in attachement :

Network key value: bfb49db8ead579a9470461697fe1bda4

Network ID filter: wpan.dst_pan == 0xfabb

It looks like a specific case linked to your gateway. Teams can’t investigate further without a ZigBee capture coming from your gateway

Have a good day,

Leslie – Community Manager

Images:
You must be logged in to view attached files.

Hi
network key
01:03:05:07:09:0B:0D:0F:00:02:04:06:08:0A:0C:0D

wpan.dst16 == 0xca08

I reupload in zip

Images:
You must be logged in to view attached files.

Hello Clément,

The provided ZigBee capture is too short to be correctly analyzed : only 20 seconds and just the first OTA launch. Also, it seems to be taken on Gateway side but far away from the ZigBee device (or with a sniffer not efficient enough ?). We see 0 messages coming from the ZigBee device (wpan.src16 == 0xca08 -> gives zero message) and finally we don’t see any OTA invalid image frame

Teams will need a more complete image if you want them to check what happens

Have a good day,

Leslie – Community Manager

Hi i reupload with sniffer short from the coordinator and the end devices
wpan.addr16 == 0xd3eb
Same key
i dont need a long capture because the time for the update failed its from the beginning

i have repeat 3 times the upgrade for more data

Images:
You must be logged in to view attached files.

as you can see the
frame
932

Command: Upgrade End Request (0x06)
Payload
Status: Ota Invalid Image (0x96)
Manufacturer Code: Vantage Controls (0x1021)
Image Type: Manufacturer Specific (0x0011)
….

Viewing 13 posts - 1 through 13 (of 13 total)

You must be logged in to reply to this topic.

Information

12 replies
2 participants