574201 / 4003C NLL Not turning on without load
Hi,
This may be an odd one, but I’d like to use the wired switch with neutral as a wireless switch, so that I don’t need to remember changing the batteries.
My plan was to:
- Add a wired switch to the actual lights (this works well)
- Add a wired switch just connected to Live and Neutral
- Create a Zigbee group for the two so that I can trigger the lights from either switch, and see whether they’re on or not using the LED (led_if_on enabled)
However, the 2nd piece doesn’t seem to work – without a load on output 1, it seems that “turning on” the switch does nothing. It remains as off on Zigbee and the LED won’t turn on. It seems like the switch is aware of whether there’s a load or not?
Is there any way to allow the switch to work without a load?
Any other ideas?
Thanks
Or if I were to place a resistor between 1 and N to have a minimal load, is there a minimum power threshold that needs to be reached?
Viewing 3 posts - 1 through 3 (of 3 total)
You must be logged in to reply to this topic.