Forum

Browse topics, discover Works With Legrand community!

CEN+ in Home + Project

<p>Hello,</p><p>Is it possible co configure CEN+ in Home + Project, and if yes how to do it?</p>

Hello,

There is only one way to configure a button as CEN+ in Home + Project :

1. Create a new scenario

2. Add the required actions to the scenario

3. Add a button as a trigger for the scenario – this button will be configured as CEN+

This is the only method currently supported by H+P to configure a button as CEN+

Have a good day,

Leslie – Community Manager

<p>Hello, I am using F461 witch doesn’t have  scenario in Home + Project, But I would like to do integration witch third party system using CEN+. Is there any other way to do this?</p>

I asked the question but didn’t had a feedback yet. I’m off next week, so I hope to get an answer at my return 🙂

Have a good day,

Leslie – Community Manager

Hello,

Here is the answer from the support :

Apologies for the previous incorrect answer

You are right: the F461 does not support scenarios. Therefore, it is not possible to configure a CEN+ button using H+P with this device

The only available workaround is to configure the button on a different system where an F460 or MHS1 is present, and then move it to your installation with the F461

Alternatively, you can use MyHome Suite, but in this case a compatible gateway will be required for the configuration

Unfortunately, there are no other solutions available at the moment

Have a good day,

Leslie – Community Manager

<p>Hello, I can confirm that you can program using F461 and MyHome Suite. Is there any plan to support this in Home+Project, because this is essential for integrating third party systems? </p>

Hello,

At this stage, it’s not yet in the roadmap of Home + Project. They think about adding this feature but it will not be soon

Have a good day,

Leslie – Community Manager

Viewing 7 posts - 1 through 7 (of 7 total)

You must be logged in to reply to this topic.

Information

6 replies
2 participants