Forum

Browse topics, discover Works With Legrand community!

Legrand Gateway – Zigbee 3.0 – Zigbee Lights

Hi,

I was looking at Zigbee 3.0 integration in Legrand products & H+C app, but I think I’ve been doing something wrong.

From what I understand and read in this forum, with Gateway on v209 we can now add third-party Zigbee 3.0 Lights to the Gateway and see them in H+C app (and by extension in Homekit).

However, if I push the EZ button on gateway (or an unpaired wireless remote), I do not get the “solid magenta” light which I should get here, only the usual green light which shows that the Gateway is ready for pairing with a Legrand product. I’m trying to pair a Philips Hue LightStrip Plus v4, so with Zigbee 3.0.

Gateway version: 209
Wireless switch version: 50
Home/away switch version: 54

Everything should be Zigbee3.0 ready, yet I cannot manage to connect to another Zigbee device.

Thanks!

Fred

Ah update, I now managed to connect the lightstrip to the Gateway, the wireless switches work well, though it is a bit unstable:

  • Just now, the light started to blink for no obvious reason, but stabilised once I gave a command via wireless switch.

Seems good, I’ll need to test a bit more!

Viewing 2 posts - 1 through 2 (of 2 total)

You must be logged in to reply to this topic.