Forum

Browse topics, discover Works With Legrand community!

problem with adding buttons and adressing

Hi,

I want to add special control H4651M2 to F411U2 actuator but I can control via app only(app  Home+Project shows that both devices are connected to the particular light). When I am pressing the button  nothing is happening.

It started to happen  since the migration from MyHomeUP app.

I have two other actuators and there is the same situation.  It seems that every new actuator is adressed xxx, 0.      (2,0;  4,0; 5,0)

I changed addresses using MyHomeSuite to 2.12; 4,12; 5;12. Unfortunately, when adding light through Home+Project, the system changed the addressing back to 2.0; 4;0 and 5.0 for individual actuators.

I did the same for only one actor (5.0 ->5.12) but the system automatically changed the address 5.12->7.0.

Regards

Adam

 

<span style=”color: rgba(0, 0, 0, 0); font-family: sans-serif; font-size: 30px; white-space: pre;”>Special control</span>

Viewing 1 post (of 1 total)

You must be logged in to reply to this topic.