More than simple construction site containers, MILA Modulaire provides living bases to the BtoB market. Connected devices from the Wiring devices “… with Netatmo” range enhance these temporary installations by providing comfort to users. The different modules are designed for the long term by being reusable as much as possible
Connected containers to improve comfort and efficiency on construction sites
MILA Modulaire has developed an application that allows them to manage energy consumption, reduce energy costs, and reduce their carbon footprint
A simple 4G router can insure the communication between all connected devices from the installation and the Cloud. Legrand’s connected devices can easily be installed according to the specific needs and the installation can be completed later to fit any other use case
Legrand will provide all connected appliances to manage electrical heating via connected outlets and dry contact DIN modules. The lighting part will be managed by micromodules linked to wireless batteryless switches
Also, these connected modules can fit other needs like provisional work places or housing, reception centers, and so on
About MILA Modulaire
French manufacturer of modular constructions since 2018, MILA Modulaire rents and sells construction site bungalows to builders, local authorities and companies. They study each partner’s request in order to offer them the ideal personalized solution corresponding to their needs. Thanks to IoT, each building can be managed locally or remotely