Classe 300X13E and SIRI
Hi all,
I have just installed Classe 300X13E and download Door Entry to my Iphone to open my gate.
I wonder if I could open the gate by using Siri.
With Siri I can open the app Door Entry but I’m not able to activate the comand to open the gate.
Thanks for your help
Floriano
Hi Leslie, all,
can we have an official ETA on this request, is there hope for a future implementation ?
I know that homekit integration will never happen (Apple requires to have bidirectional communication with the device which is not possible). However Siri shortcuts is possible.
On my side I found a workaround but it is not satisfying at all : I bought a connected bridge from Somfy (Tahoma) which lets communicates with my gate through RTS protocol. But I learned that Siri shortcuts are not implemented either and homekit is not possible either. So I ended up with the supported IFTTT plugin that lets me send a voice command to open the gate remotely… so complicated….
Just sharing my experience to explain that this feature is still a must have. Thanks
Hi Damien,
Can you explain me, how have you integraded your door entry Classe 300X13E into somfy tahoma – you wrote you communicates over RTS protocol ….
THX
Florian
Hi,
I purchased this unit : Somfy 1841022 which is a RTS receiver. I plugged it in the same way as the legrand switch to the motherboard of the gate.
Once plugged in, launch detection from the Tahoma app (I had issues with distance (~20 meters) as the gate if far from the tahoma, I added an external antenna and it works now)
Then this receiver acts as a RTS relay with 2 entities (wired to the open and close commands on the motherboard of the gate).
But this is not enough : Tahoma app won’t allow siri shortcuts and this device won’t integrate into homekit.
So this is the last step with 2 possibilities :
1/ Tahoma allows IFTTT integration : then you can configure voice commands or better geofencing to open the gate when you arrive in the zone
2/ Use a domotic system such as Home assistant that has a tahoma plugin
Hi,
Thanks for your detailed explanation. To modify the motherboard on the gate is not an option in may case. SIRI is not so important for me – it would be nice only to open and close the door.
Anyway, it seems i have to wait until the API is working again for Classe300X13E – hopefully it will be solved from netatmo soon… again, for me it’s absolutly ununderstandable to remove a service before the new one is in place…
Thanks a lot!
Flo
Actually this is not a modification of the board : when you wired the classe300 to your gate, you probably wired the provided bticino module (an orange module) which acts as a relay between your BTICino street plate and the motherboard of the gate. What I did is just add the somfy module, wired exactly the same as the bticino module to the motherboard.
I don’t know if any API will work one day for this model…
i didn’t do the installation by myself. So i want touch it.
Yes, there was an API in the past – but is depreciated and netatmo must add the class300 to their infrastructure. in an other Thread the moderator told me, that this will be done … bu nobody knows when
Thanks a lot again!!
br
Flo
Thanks Leslie for the replay. What is the F454 you mention in my reply?
How could I find out which models my video door bell is? Can you tell it from a picture?
And, is there a compatible replacement to make it work with homekit?
Hi Michele,
A F454 is a webserver from MyHOME solution you can find in your electrical panel. It makes the connection with your video entry system via SCS protocol and permits the remote access to it : https://catalogue.bticino.com/BTI-F454-EN
The photo you sent me is just the entrance panel which is a “dumb” device
The only videophone solution we have with a HomeKit compatibility is the Netatmo Doorbell but I don’t know if it could fit your needs
I strongly advise you to contact the Customer Support of your country to get information and help about the compatibility
Have a good day,
Leslie – Community Manager
You must be logged in to reply to this topic.