Door Entry App Migration in H+S App
Hi,
When will the Door Entry app be migrated to the Home + Security app? it has been many years. Below are the product codes that are not migrate
BT-344682, BT-344932, BT-344786: Door Entry CLASSE100X
BT-344642, BT-344643: Door Entry CLASSE300X
BT-3488, BT-3488W, LG-067259: Door Entry for HOMETOUCH
BT-318011/12/15, LG-369420/30, BT-332851/52/55, LG-369425/35: Door Entry EASYKIT
A funny thing integration with the Legrand system is that
MHserver1 & F460 New Web Server can be Control Home + Control App
Home Touch 3488 Can Be Control Door Entry App
Bugler Alarm System 4200C Can Bed Control Home + Security .
This is like Smart Home System ? 3 apps ?
Hello Sumit,
Concerning the C300X + HomeTouch, it’s not planned to migrate them to Netatmo’s infrastructure. So, these devices will stay only available on their dedicated app
Concerning the C100X, C100X “… with Netatmo” devices work with Home + Security app. The devices that will not be migrated were produced before these dates :
344682 23W23
364614 23W22
For EasyKit, I put below the references of migrated devices :
| BT-310913 | LG-360910 | EASYKIT Wifi with Netatmo 2 wire with 7″ monitor and entrance panel with color camera. PLUG-IN power supply included. |
| BT-335253 | LG-365220 | EASYKIT Wifi with Netatmo 2 wire 7″ additional monitor. PLUG-IN power supply included. |
| BT-310914 | LG-360915 | EASYKIT Wifi with Netatmo 2 wire with 7″ monitor and entrance panel with color camera. DIN power supply included. |
| BT-335254 | LG-365225 | EASYKIT Wifi with Netatmo 2 wire 7″ additional monitor |
Have a good day,
Leslie – Community Manager
<span style=”color: #545354; font-family: ‘Source Sans Pro’, sans-serif; font-size: 18px;”>Concerning the C300X + HomeTouch, it’s not planned to migrate them to Netatmo’s infrastructure. So, these devices will stay only available on their dedicated app</span>
Ok, but how can I interact with the system then if the Work wih Legrand API has been powered off?
https://portal.developer.legrand.com/apis
Is there a way to control the device locally via Open Web Net via Local interoperability?
Thanks
Giulio
Hello Giulio,
I’m stuck too, I have a C100X and I’m tryin to figure out how to interact with it, even if only local.
Waiting for Leslie too.
Hello Giulio & Davide,
OpenWebNet local protocol is only available for MyHOME system (https://developer.legrand.com/solutions/myhome/)
As said previously, there is unfortunately no way to interact with C300X and non-migrated C100X via the former Cloud API nor in a local way. These devices can only be used via their respective native apps
Have a good day,
Leslie – Community Manager
It’s a decision that I do not understand also because the device is the last to have been developed while previous models have been migrated.
If I had known, I would not have invested my money in the MHS and Hometouch combination.
Knowing now that I can replace both with a single 300EOS is truly saddening.
Regards
Giulio
You must be logged in to reply to this topic.