MHS1 and new app Home+Control
Some days ago my HMS1 has lost its fixed ip address during night, falling to dhcp address so it was no more reachable from Openhab portal that integrates Bticino bus with other devices in my home. I tried to reset it with MyHomeUP with installer code app but I could not reset the old fixed ip, it always restarted with dhcp address. So, reading somewhere in internet I found that the the old app MyHomeUp was no more updated. They suggested to move to the new app Home+Control. I did this and the new app can reach the server, but now I have lost completely the old app (it says that mhs1 is no more reachable) and the new app does not allow the installer access but only the normal user access. So I do not know how to manage my MHS1 and neither i cannot rollback to previous configuration. My old scenarios are still active but I cannot disable or edit or delete them because they belong to installer. The app says to call the installer … but I have installed it myself!
Please help me!
Enrico, which firmware did you use? Can you send me a link or file?
Hi all,
I configured myhomeserver1 through Home+Project and everything seems ok, but when try to use Home + Control with the user code, it always says “Device already installed”, and the owner of the house must make you guest.
I’m stuck in this situation, is there any chance to unlock this or to (hard) reset the gateway?
Hi all,
I’m having an issue with accessing my H+C. In my house, I have a Bticino MyHOME_Up server, and for configuration, I’m using H+P (version 1.0.16), which is still accessible through the android app.
Since the latest version of H+C (2.13.4.0) I cannot access my setup anymore. Is anyone else experiencing the same issue?
Thanks in advance,
@Leslie – Community Manager can you help us here. I’m hopeless / my Home + Control is useless as I wrote in the previous msg. Thanks
Hello simonjaz,
I can’t be helpful on this point. You must contact directly the Customer Support of your country, they will know what to do to help you
Have a good day,
Leslie – Community Manager
hi all,
i was able to solve my problem thanks to this FB group i found on internet.
Maybe this can help you.
Hi all,
I managed to solve this problem with customer support. They updated my FW remotely. So now it finally works. Best
<span style=”color: #575757; font-family: ‘Segoe UI’, ‘Noto Sans’, sans-serif;”>I also upgrade to the new (“better”) Home Control app but lost a lot of features</span>
<span style=”caret-color: #050505; color: #050505; font-family: system-ui, -apple-system, BlinkMacSystemFont, ‘.SFNSText-Regular’, sans-serif; font-size: 15px; white-space: pre-wrap;”>Does anyone else have Problems configuring HC/HS/HD4658 PIR+US flush mounted sensors? Although they can successfully be configured with H+P they always get the address A0:P1 and not the correct address of the linked light actor?</span>
Just to share that i found help here, it’s a great comunity that i found on facebook.
https://www.facebook.com/groups/356185239047894
from this thread I feel like buying up old F454 is the better way to go for now… until this cloud stuff goes away…
as for “the device lost it’s IP address”, the better way to solve this is to program your home router to assign the same exact IP address to your MHS1 when presented with it’s mac address, which is on the sticker somewhere.
I have MyHomeserver1 firmware 3.83.04 installed and the Home+Control application 3.0.5.0. When I try to add the server in the H+C Application, I cannot because the application reports that the server cannot be found. Even if I enter the server’s IP address, the error remains the same. The H+P application works normally. Can you please provide instructions on what to do to successfully connect to H+C?
You must be logged in to reply to this topic.